Back to Newsroom

The Latest Trends in Surgical Power Tools Design

July 12, 2023
surgical power tools design

Surgical power tools have been a critical part of the medical industry for decades, having undergone significant advancements in recent years to meet the ever-shifting demands of surgical procedures. Rapid technological innovation has not only helped facilitate the development of more precise and efficient surgical power tools, but the continued miniaturization of the miniature motors that power these tools. Let’s explore the latest trends in surgical power tools and the qualifications to consider when searching for a motion solutions supplier to partner with when developing a new hand tool.

The Latest Trends in Surgical Power Tools Design

Innovations in technology have radically transformed how surgical power tools are designed. Let’s explore a few of the most recent trends in how these tools are designed:

  • Durability. Surgical power tools are often subjected to high stresses and extreme wear and tear; as such, they must be built to withstand these demands. The latest surgical power tools are designed with greater durability and robustness, ensuring they can withstand prolonged use without losing efficiency or accuracy.
  • Ergonomics. Ergonomics is a significant consideration when it comes to surgical power tools. These tools must be comfortable for surgeons to hold and operate for extended periods to avoid fatigue and discomfort. New surgical power tools are being designed with ergonomics in mind, including features such as adjustable grips and lighter weight.
  • Robotics. With robotic-assisted surgery, the surgeon uses a robotic arm to perform the procedure with the assistance of a 3D camera and a computer system. This type of surgery allows for greater accuracy and precision, which can result in improved patient outcomes. Surgical power tools are being developed to integrate seamlessly with robotic systems and have become increasingly popular in recent years.
  • Minimally Invasive Surgery. Minimally invasive surgery has gained significant popularity in recent years as it offers several advantages over traditional open surgery. With minimally invasive surgery, surgeons can perform procedures using small incisions, resulting in less scarring, reduced blood loss, and a shorter recovery time for patients. To cater to this trend, surgical power tools are designed to be smaller and more precise, with enhanced maneuverability.

Selecting a Motion Supplier for Surgical Power Tools Design

One of the most critical milestones when designing a surgical power tool is selecting a miniature motor provider. This supplier is not only essential in providing the motion solutions powering the device, but can also help ensure that the device is fully optimized from the outset. A key consideration when choosing a supplier is that they offer a wide range of motor technologies and accessories. Related to this is their ability to customize the motion solution in order to meet the specific needs of a new surgical power tool; customization features can include torque, speed, autoclavability requirements, and motor size. A second consideration is the supplier’s commitment to quality and innovation, while a third is their reputation and history in designing solutions for this application. A global network of sales and engineering locations should also be taken into account.

One supplier that matches all of the above qualifications is Portescap. A leading motion solutions provider with extensive experience in designing and manufacturing motors for surgical power tools like hand-held drills, saws, reamers, and shavers, our expertise in motor design lets us easily guide surgical hand tool manufacturers on the ideal motor for their new surgical power tool. Likewise, our dedication to innovation means that manufacturers partnering with us can be confident that they have chosen a supplier that is continually looking for ways to improve its products. We also invest heavily in research and development to ensure that our motors are at the forefront of technological advancements in the industry.

The latest surgical power tools offer greater precision, efficiency, and durability than those of the past. With the increasing demand for minimally invasive surgery and robotic-assisted surgery, there is a growing need for devices that are smaller, more precise, and can easily integrate with robotic systems. Portescap’s motors are renowned for their precision, efficiency, and durability, making us a natural choice for companies looking to develop new surgical power tools with the above requirements. Reach out to us here – our engineers are ready to assist!