Browse News Categories
Additional Resources
Common Questions When Evaluating Motion Solutions for Cardiovascular Devices

When engineers begin designing a cardiovascular device, they're faced with a slew of decisions, each crucial for the device's success. Among these, choosing the right motion solution takes center stage, as it's the powerhouse driving the device's core functions. Keep in mind that it's not just about powering the device; the miniature motion system shapes the entire device’s performance, lifespan, and overall effectiveness. Engineers need to dig deep, ensuring that their chosen motion components align perfectly with their project's unique goals and needs. Here are a few essential considerations to help you select the perfect fit for your cardiovascular project:
- Motor:
- How does the motor diameter and length impact the output performance?
- Which brushless DC technology meets the speed profile required?
- What technology is most suited to the rapid acceleration my device needs?
- How do I balance the motor selection with the number of operational cycles for the device?
- Gearbox:
- What is the output speed required from the device and how does the gearing selection influence that parameter?
- What gearing technology is best suited for high motor speeds?
- What is the life requirement for the device and which gearing technology is best aligned?
- Encoder:
- What resolution is needed to monitor the speed of the motor relative to the device requirements?
- Does the feedback solution need to withstand device handling and drops?
- Do I need an encoder, or can a code wheel meet the device needs?
In the world of cardiovascular device development, nailing the motion solution is key to success. By tackling the questions outlined above, engineers can navigate this crucial aspect with ease and precision. Ready to tap into Portescap's expertise in motion system design? Our engineers are always ready to assist! Let's propel your project towards excellence and innovation together.