Browse News Categories
Additional Resources
Understanding Gearheads: Applications and Selection

A gearhead, also known as a gear reducer, gearbox, or enclosed speed reducer, is a mechanical device used to increase the output torque or change the speed (RPM) of a motor. This blog dives into the types of gearheads, their applications, and how to select the right one for your needs.
What is a Gearhead?
Gearheads are essential components in many electromechanical drive systems. They are used in various applications, including machine tools, industrial equipment, conveyor belts, and virtually any power transmission system with rotary motion that requires a change in torque and speed. There are two main types of gearheads: spur compound gearheads and planetary gearheads. You can explore the in's and out's of each technology here.
Exploded views of a spur compound gearhead (left) and planetary gearhead (right)
Why is a Gearhead Needed?
A motor alone has limited capacity to transmit torque and power. A gearhead enhances the motor’s capacity to perform and sustain higher torque.
Here are several reasons why a gearhead is necessary:
- Speed and Torque Conversion. A gearhead allows the motor to operate at its optimal speed and torque levels by changing the output speed and torque ratio as needed for a specific application. This ensures the motor can efficiently drive the load it is connected to.
- Mechanical Advantage. A gearhead provides a mechanical advantage by increasing or decreasing the output speed and torque compared to the motor's input. This allows the motor to generate more power or sustain higher torques than it would be able to on its own.
- Control and Flexibility. Using a gearhead gives the operator greater control over the speed and torque of the motor, making it adaptable to a wide range of applications. This flexibility is essential for various industrial processes and machinery.
- Durability and Longevity. A gearhead reduces the wear and tear on the motor by allowing it to operate within its optimal speed and torque ranges. This can extend the motor's lifespan and reduce maintenance and repair costs in the long run.
Overall, a gearhead is essential for optimizing the performance, efficiency, and durability of a motor in various applications, including industrial power tools, medical infusion pumps, surgical motion solutions, and robotics.
How to Select a Gearhead
Selecting the right gearbox for a specific application involves considering various factors:
- Load Requirements. Determine the torque, speed, and power needed for the application to select a gearbox that can handle the load requirements effectively. Generally, for higher torques and compact solutions, a planetary gearbox is preferred. For comparatively lower torque and higher efficiency or quieter applications, a spur compound gearbox is ideal.
- Space Constraints. Miniature gearboxes are compact and space-saving. It is important to consider the physical size constraints of the application and choose a gearbox that fits within the available space. If the application demands an intricate shape and size, a spur compound gearbox is preferred. If straight space is available, a planetary gearbox can help carry higher torques and is comparatively robust in its construction.
- Gear Ratio. The gear ratio of the gearbox will determine the output speed and torque of the system. Choose a gearbox with the appropriate gear ratio for the desired output.
- Efficiency. Consider the efficiency of the gearbox to ensure minimal power loss during operation.
- Operating Environment. Consider factors such as temperature, humidity, and potential exposure to contaminants when selecting a gearbox to ensure it can withstand the conditions of the application.
- Mounting Options. Consider how the gearbox will be mounted in the application and choose a gearbox with the appropriate mounting options for easy installation.
- Cost. Consider the budget constraints of the application and choose a gearbox that offers the best value for the price.
Conclusion
Gearheads play a critical role in enhancing motor performance, efficiency, and durability. Understanding the types, applications, and selection criteria can help you make informed decisions to optimize your electromechanical drive systems. Having difficulty in determining which type of gearhead is right for your unique application requirements? Reach out to our engineers here to discuss!