Browse News Categories
Additional Resources
New Applications and Trends Revolutionizing Surgical Robotics

Surgical robotics continues to revolutionize the world of surgery, with the use of robotic technology in surgical procedures allowing for greater precision, reduced risks, and faster recovery times. These systems are becoming even more advanced due to evolving technology, with new applications and changing surgical trends emerging at a rapid pace. Let’s explore these industry shifts, as well as examine why motion control, particularly micro motion, is crucial to the advancement of surgical robotics.
New Applications and Trends in Surgical Robotics
Surgical robotics systems have traditionally been used in three types of surgeries: 1) minimally invasive surgeries; 2) catheter-based surgeries; and 3) open surgeries. Minimally invasive surgeries are performed with tiny incisions that allow for minimal blood loss and faster recovery times, while catheter-based surgeries involve the use of a small tube that is inserted into the patient's body through a small incision. Open surgeries, meanwhile, utilize larger incisions and more invasive procedures.
Surgical robotics systems are used to perform all three of these surgery types, though it's critical to note that due to evolving surgical technology, innovative applications of surgical robotics systems are also under development. These include:
- Surgical procedures in hard-to-reach areas of the body, such as the brain and spinal cord
- Surgical procedures on delicate structures such as the eyes and ears, where even the slightest movement or deviation can have severe consequences
- Surgical procedures on newborns, who require much smaller incisions and more delicate procedures
There is also an emerging trend of using both autonomous systems and augmented reality in surgical robots. Autonomous systems use artificial intelligence (AI) to analyze data and perform certain tasks without human intervention; this technology is particularly beneficial in surgical procedures that require precise movements and calculations. Augmented reality (AR) allows surgeons to see inside the patient's body in real-time, providing essential information during the surgery.
How Micro-Motors are Advancing Surgical Robots
Motion control, particularly micro motors, is a crucial component in the advancement of surgical robotics. Micro motors are miniature motors that are responsible for controlling the movement of surgical instruments and cameras in the surgical robotics system. The use of micro motors has helped to revolutionize this field, allowing for faster recovery times and improved patient outcomes; enhancing the surgical robot’s dexterity; and facilitating heightened precision and more controlled movement in surgical procedures.
As technology continues to evolve, we can expect to see even more impressive applications of surgical robotics systems and further advancements in the field. Portescap’s engineers are ready to assist with the development of your next surgical robotics project – reach out to us here to start collaborating!