Experience Portescap’s Comprehensive Motion Solutions at The Assembly Show

Portescap, a trusted brand and provider of motion solutions for assembly and automation, is excited to announce its participation in The Assembly Show 2024. The event will take place from October 22-24, 2024, at the Donald E. Stephens Convention Center in Rosemont, Illinois. Attendees can visit Portescap at Booth 444 to explore their innovative solutions designed to enhance efficiency and performance in various industrial applications, including battery-powered hand tools, pick and place, and materials handling.

A key highlight during the show will be Portescap’s ECF brushless DC slotted flat motors series, which are well-suited for demanding applications with varying operating profiles. The ECF series offers diameters ranging from 20mm to 90mm and is perfect for applications where space is limited and performance demands are high. Their compact, flat form factor with high-power density ensures higher load capacity without speed loss while producing a smooth output torque and enhanced efficiency.

Portescap will also be presenting its broader range of BLDC, brush DC, and stepper motors, demonstrating their versatility and capability in meeting diverse motion control requirements.

As part of the Regal Rexnord family, Portescap leverages a wealth of resources and expertise to deliver cutting-edge solutions to its customers. The company is dedicated to a systems approach, focusing not just on individual motors or motion accessories, but on how each component integrates into the larger system. This holistic perspective ensures that every element supports optimal performance and efficiency and aligns perfectly with Regal Rexnord’s systems approach.

For more information on Portescap’s portfolio of miniature motion solutions, please visit www.portescap.com or email [email protected].